FB#.RESREFPHASE

Description

This parameter sets the electrical degrees of phase lag in the resolver.

See the motor resolver datasheet for the value for this parameter.

Context

See Feedback Settings.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

electrical degrees

Range

-180 to 180°

Default Value

-2°

Data Type

Float

See Also

N/A

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

Fieldbus Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCAT COE and CANopen FB1.RESREFPHASE 0x3500 0x5 UDINT - - RW False
FB2.RESREFPHASE 0x3501 0x5 UDINT - - RW False
FB3.RESREFPHASE 0x3502 0x5 UDINT - - RW False
FB4.RESREFPHASE 0x3503 0x5 UDINT - - RW False
FB5.RESREFPHASE 0x3504 0x5 UDINT - - RW False