FB#.SINGLETURNBITS

Description

Number of single turn bits used for BiSS rotary encoders. Feedback data sheet specifies the number required.

Context

Only used for when FB#.MECHTYPE is rotary and identified feedback is BiSS. See Feedback Settings.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

single turn bits

Range

1 to 32

Default Value

19

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.