AXIS#.SAFE.SLI_#.INTERNALSTATE

Description

Indicates the internal state of the Safely Limited Increment (SLI) function state machine.

Value Description

0

Initial

1

Not Running

2

Monitoring

3

Fault Reaction

4

Delay Before Monitoring

State Machine Diagram

Context

For complete SLI information refer to SLI (Safely Limited Increment).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read only

Units

N/A

Range

0, 1, 2, 3, 4

Default Value

N/A

Data Type

Integer

Stored in Non-Volatile Memory

No