AXIS#.SAFEPARAM.SLI_#.FAULTREACTION

Description

Indicates the safety function activated when the Safely Limited Increment (SLI) safety function is faulted. The parameter uses one of the following values:

Value Description

1

STO

2

SS1 Instance 1

3

SS2 Instance 1

 

Parameters Editor with Fault Reaction values circled

Context

For complete SLI information refer to SLI (Safely Limited Increment).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

1, 2, 3

Default Value

1 (STO)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLI_1.FAULTREACTION

3169h

07h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLI_2.FAULTREACTION

316ah

07h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLI_3.FAULTREACTION

316bh

07h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLI_1.FAULTREACTION

3269h

07h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLI_2.FAULTREACTION

326ah

07h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLI_3.FAULTREACTION

326bh

07h

Unsigned8

-

-

Read/Write

No