AXIS#.SAFEPARAM.SAR_#.FAULTREACTION

Description

Indicates the safety function activated when the Safe Acceleration Range (SAR) safety function is faulted. The parameter uses one of the following values:

Value

Description

1

STO

2

SS1 Instance 1

3

SS2 Instance 2

 

Context

For complete SAR information refer to SAR (Safe Acceleration Range).

Related safety parameters:

Versions

Action Version Notes

Implemented

02-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

1, 2, 3

Default Value

1 (STO)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SAR_1.FAULTREACTION

3166h

06h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SAR_2.FAULTREACTION

3167h

06h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SAR_3.FAULTREACTION

3168h

06h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SAR_1.FAULTREACTION

3266h

06h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SAR_2.FAULTREACTION

3267h

06h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SAR_3.FAULTREACTION

3268h

06h

Unsigned8

-

-

Read/Write

No