WorkBench Interface: Toolbar
The WorkBench Toolbar provides several convenient features.
|
Element | Function |
---|---|
Navigation | These buttons let you navigate through the history of views you have accessed, or jump up one level of nested views. See WorkBench Interface: Navigation for more information. |
Watch Window | This button opens the Watch window. See Watch for more information. |
Panic | This button immediately disables all devices. |
Functions | Disable drive and clear faults; save parameters to NVRAM; start or disconnect communication with the selected device. |
Axis Control | These controls allow you to enable/disable, stop any motion, and set the axis' Command Source and Operation Mode. There are independent controls for each axis. See Axis Settings for more information. |