WHEN.PLFB
Description
Records the value of Position when the when-condition is satisfied. The when-condition is checked once per 250 microseconds.
General Information
Type |
R/O |
Units |
Depends on UNIT.PROTARY or UNIT.PLINEARUNIT.ACCLINEAR Rotary: counts, rad, deg, (Custom Units), 16-bit counts Linear: counts, mm, µm, (Custom Units), 16-bit counts |
Range |
N/A |
Default Value |
N/A |
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
---|---|---|---|---|---|
Modbus |
1178 |
Yes | 64 bit | Yes |
M_01-05-11-000 |
Related Topics