MC_RemAxisFromGrp
Function Block A function block groups an algorithm and a set of private data. It has inputs and outputs. - Removes an individual axis from an axis group.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
Execute |
BOOL |
0, 1 |
N/A |
No default |
On the rising edge The transition of a digital signal from low to high. AKA: positive edge., request to remove an axis from the group. |
AxesGroupRef |
No range |
N/A |
No default |
The axis group from which the axis is removed. |
|
IdentInGroup |
UINT |
0, MaxNumberOfAxes - 1 |
N/A |
No default |
The zero-based index Zero pulse (zero signal) of a hardware pin such as digital input or feedback pin. of the axis in the group.
|
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Done |
BOOL |
|
|
If TRUE, the command completed successfully. |
Error |
BOOL |
|
|
If TRUE, an error has occurred. |
ErrorID |
INT |
|
|
Indicates the error if Error output is TRUE. |
Remarks
-
- This function block starts a motion-related action and stores data for calculations and error checking.
See Call Function Blocks Multiple Times in the Same Cycle if using a dual-core controller.
- See Coordinated Motion, the top-level topic for Coordinated Motion.
- This function or function block does not generate any motion.
- This function block can be issued in the group states: (GroupDisabled, GroupStandby, or GroupErrorStop).
- The group’s state changes to GroupDisabled if the axis removed is the last valid axis in the group.
- MC_RemAxisFromGrp fails if the group is in any state other than GroupStandby or GroupDisabled.
- See Group State Diagrams.
Figure 1: MC_RemAxisFromGrp
FBD Language Example
FFLD Language Example
IL Language Example
BEGIN_IL Instruction list - This is a low-level language and resembles assembly.
CAL Inst_MC_RemAxisFromGrp( ExecuteRemAxisFromGrp, Group1_Ref, AxisId )
END_IL
ST Language Example
(* Inst_MC_InitAxisGrpST example *)
Inst_MC_RemAxisFromGrp( ExecuteRemAxisFromGrp, Group1_Ref, AxisId );
See Also