MC_KIN_REF Structure
The MC_KIN_REF structure defines the robotic system transform type and its parameters.
The parameters are specific to each transform type.
General MC_KIN_REF Structure
Member |
Data Type |
Description |
|
---|---|---|---|
TransformType |
UINT |
A number that identifies the specific robotic system transform. The #defines for the transform types are: |
|
KinParameters [0 - 31] |
LREAL |
|
Robotic Transform Parameters
- These parameters must be specified for all ACS Axes Coordinate System - The system of coordinates related to the physical motors and the single movements caused by the single drives. axes in the AxisGroup.
- There are two parameters for each ACS axis.
MC_TRANSFORM_TYPE_GANTRY
Figure 1: MC_TRANSFORM_TYPE_GANTRY
Parameter Count |
Parameter # |
Description |
Range |
---|---|---|---|
1 |
MC_GANTRY_KIN_PARAM_REVERSE_X |
Reverse X-axis. |
|
MC_TRANSFORM_TYPE_GANTRY_WITH_SKEW
Figure 2: MC_TRANSFORM_TYPE_GANTRY_WITH_SKEW
Parameter Count |
Parameter # |
Description |
Range |
---|---|---|---|
3 |
MC_GANTRY_WITH_SKEW_KIN_PARAM_REVERSE_X |
Reverse X-axis. |
|
|
MC_GANTRY_WITH_SKEW_KIN_PARAM_SKEW_SCALE |
Skew to linear unit ratio. |
|
|
MC_GANTRY_WITH_SKEW_KIN_PARAM_REVERSE_SKEW |
Reverse Skew-axis. |
|
MC_TRANSFORM_TYPE_HBOT
Figure 3: MC_TRANSFORM_TYPE_HBOT
Parameter Count |
Parameter # |
Description |
Range |
---|---|---|---|
3 |
MC_HBOT_KIN_PARAM_LIN_TO_ROT_RATIO |
Linear to rotational unit ratio. Example: cm/degree. |
Positive value. |
|
MC_HBOT_KIN_PARAM_REVERSE_X |
Reverse X-axis. |
|
|
MC_HBOT_KIN_PARAM_REVERSE_Y |
Reverse Y-axis. |
|
MC_TRANSFORM_TYPE_TBOT
Figure 4: MC_TRANSFORM_TYPE_TBOT
Parameter Count |
Parameter # |
Description |
Range |
---|---|---|---|
3 |
MC_TBOT_KIN_PARAM_LIN_TO_ROT_RATIO |
Linear to rotational unit ratio. Example: cm/degree. |
Positive value. |
|
MC_TBOT_KIN_PARAM_REVERSE_X |
Reverse X-axis. |
|
|
MC_TBOT_KIN_PARAM_REVERSE_Z |
Reverse Y-axis. |
|
MC_TRANSFORM_TYPE_DELTA (*Experimental*)
Figure 5: MC_TRANSFORM_TYPE_DELTA (*Experimental*)
Parameter Count |
Parameter # |
Description |
Range |
---|---|---|---|
4 |
MC_DELTA_KIN_PARAM_RADIUS_BASE_LENGTH |
RadiusBaseLength |
Positive, non-zero value. |
|
MC_DELTA_KIN_PARAM_RADIUS_END_LENGTH |
RadiusEndLength |
Positive, non-zero value. |
|
MC_DELTA_KIN_PARAM_MOTOR An actuator focused to a movement, converting electrical energy in a force or torque._ARM_LENGTH |
MotorArmLength |
Positive, non-zero value. |
|
MC_DELTA_KIN_PARAM_END_ARM_LENGTH |
EndArmLength |
Positive, non-zero value. |
MC_TRANSFORM_TYPE_SCARA_ELBOW_POS (*Experimental*)
Figure 6: MC_TRANSFORM_TYPE_SCARA_ELBOW_POS no Wrist |
Figure 7: MC_TRANSFORM_TYPE_SCARA_ELBOW_POS with Wrist |
Parameter Count |
Parameter # |
Description |
Range |
---|---|---|---|
2 or 3 The parameter count depends on the axis number of the AxisGroup.
|
MC_SCARA_KIN_PARAM_UPPER_ARM_LENGTH |
RobotUpperArmLength |
Positive, non-zero value. |
|
MC_SCARA_KIN_PARAM_LOWER_ARM_LENGTH |
RobotLowerArmLength |
Positive, non-zero value. |
|
MC_SCARA_KIN_PARAM_WRIST_LENGTH |
RobotWristLength Available for SCARA with wrist only. |
Positive, non-zero value. |
MC_TRANSFORM_TYPE_SCARA_ELBOW_NEG (*Experimental*)
Figure 8: MC_TRANSFORM_TYPE_SCARA_ELBOW_NEG no Wrist |
Figure 9: MC_TRANSFORM_TYPE_SCARA_ELBOW_NEG with Wrist |
Parameter Count |
Parameter # |
Description |
Range |
---|---|---|---|
2 or 3 The parameter count depends on the axis number of the AxisGroup.
|
MC_SCARA_KIN_PARAM_UPPER_ARM_LENGTH |
RobotUpperArmLength |
Positive, non-zero value. |
|
MC_SCARA_KIN_PARAM_LOWER_ARM_LENGTH |
RobotLowerArmLength |
Positive, non-zero value. |
|
MC_SCARA_KIN_PARAM_WRIST_LENGTH |
RobotWristLength Available for SCARA with wrist only. |
Positive, non-zero value. |