MLMotionInit
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Initializes the motion library.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
BOOL |
TRUE, FALSE |
N/A |
FALSE |
Enable function. |
|
BasePeriod |
LREAL |
Minimum: 125 |
Microseconds |
1000 |
Duration of one motion cycle.
|
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
BOOL |
TRUE, FALSE |
N/A |
|
Remarks
- Must be called before any other Motion Library function.
- Returns TRUE if the function succeeded.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Initialization code to start EtherCAT network.
//First initialize network with MLMotionInit command
//Then wait for command to finish by monitoring MLMotionStatus output
//Once initialized, create any cam profiles The position of a slave axis is mathematically linked to the position of a master axis. Example: A system where two rotating drums turn at a given ratio to each other. A more advanced case of electronic gearing is electronic camming. With electronic camming, a slave axis follows a profile that is a function of the master position. This profile need not be linear but it must be a mathematical function. and PLCopen A vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML. or Pipenetwork devices
//Then call MLMotionStart and monitor MLMotionStatus again before beginning rest of program The act of performing a sequence of instructions or commands.
FirstCycle := TRUE;
On FirstCycle DO //Initialize the motion engine
MLMotionInit( 1000);
END_DO;
MotionEngineStatus := MLMotionStatus();//Check the current status of the motion engine
//Once motion engine is initialized, create CAM profiles and defined Axis, then start the motion engine
ON MotionEngineStatus = MLSTATUS_INITIALISED DO
Profiles( MLPR_CREATE_PROFILES );
PLCopen( 0 );
MLMotionStart();
END_DO;
IF MotionEngineStatus = MLSTATUS_RUNNING THEN
bMotionEngineStarted := TRUE;
ELSE
bMotionEngineStarted := FALSE;
END_IF;