MC_StopRegist
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
En |
BOOL |
FALSE, TRUE |
N/A |
No default |
|
Axis |
AXIS_REF |
1, 256 |
N/A |
N/A |
Axis registration to turn off. |
TriggerInput |
TRIGGER_REF |
See Description. |
N/A |
No default |
Structure specifying the fast input. (to disarm) The structure elements are: Direction The orientation components of a vector in space.INT Range = 1, 5.
InputID INT Range = 0, 1
TrigidINT Range = 0, 256.
|
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
OK |
BOOL |
FALSE, TRUE |
N/A |
Execution successful. |
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller.
-
-
To use Capture Engine 1, modify the input PDOs that are used and add the Latch The control word is used to activate the drive's latch status machine. The latch control word is processed independently of the EtherCAT® bus cycle. The status word is used to return the drive's latch status. Position Position means a point in space which is described by different coordinates. Depending on the used system and transformation it can consist of a maximum of six dimensions (coordinates).This means three Cartesian coordinates in space and coordinates for the orientation. In ACS there can be even more than six coordinates. If the same position is described in different coordinate systems the values of the coordinates are different. 1 parameter.
Figure 1: MC_StopRegist
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
StopOK := MC_StopRegist( Axis1, Trig1);
See Also