MLAddInit
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Initializes an Adder Pipe Block for use in a PLC Programmable Logic Controller - A digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events. Program The act of performing a sequence of instructions or commands. with user-defined settings.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of a created Pipe Block. |
Offset1 |
LREAL |
No range |
N/A |
No default |
Sets the Offset value of the first entry of an Adder object. |
Offset2 |
LREAL |
No range |
N/A |
No default |
Sets the Offset value of the second entry of an Adder object. |
Ratio1 |
LREAL |
No range |
N/A |
No default |
Sets the Ratio value of the first entry of an Adder object. |
Ratio2 |
LREAL |
No range |
N/A |
No default |
Sets the Ratio value of the second entry of an Adder object. |
Outputs
Adder Block Output = Ratio1*Input1 + Offset1 + Ratio2*Input2 + Offset2
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
|
|
Returns TRUE if the Adder Pipe Block is initialized. |
Remarks
-
-
Adder objects are normally created in the Pipe Network using the graphical engine.
You do not have to add MLAddInit function blocks A function block groups an algorithm and a set of private data. It has inputs and outputs. to their programs.
Parameters are entered directly The orientation components of a vector in space. in pop-up windows and the code is automatically added to the current project.
- Function block is automatically called if an Adder Block is added to the Pipe Network.
- User-defined settings are entered in the Pipe Blocks Properties screen.
- The Pipe Block is assigned ratios and offsets for both inputs.
- After an Adder block is initialized, the inputs need to be selected using the MLAddWriteInput function block or graphically using the Pipe Network.
Figure 1: MLAddInit
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Create and Initiate a Trigger object
MyAdder := MLBlkCreate( 'MyAdder', 'ADDER' );
MLAddInit( MyAdder, 1.0, 0.0, 1.0, 0.0 );
See Also