MLAddWriteInput
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Sets the source of an input of an Adder Pipe Block.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of an initiated Adder object. |
InputID |
DINT |
1, 2 |
N/A |
No default |
Select first or second input to the Adder object. |
InputBlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of an initiated Pipe Block. This is an input to the Adder object. |
Outputs
Adder Block Output = Ratio1*Input1 + Offset1 + Ratio2*Input2 + Offset2
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
|
|
Returns TRUE if the input to the Adder object is set. |
Remarks
- Function block A function block groups an algorithm and a set of private data. It has inputs and outputs. is automatically called if an Adder Block is connected to other blocks in the Pipe Network.
Figure 1: MLAddWriteInput
-
-
Adder objects are normally created in the Pipe Network using the graphical engine.
You do not have to add MLAddWriteInput function blocks to their programs The act of performing a sequence of instructions or commands..
Blocks are connected with lines in the Pipe Network.
The code is automatically added to the current project.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Set the first input of an Adder pipeblock to be connected to the output of GEAR1 pipeblock
MLAddWriteInput( PipeNetwork.ADDER, 1, PipeNetwork.GEAR1 );
See Also