MLAxisGenIsRdy
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Verifies if an axis is ready.
Specifies whether the Axis generator is ready.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
ID |
DINT |
No range |
N/A |
No default |
ID Name of the Axis block. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE when the function successfully executes. |
Remarks
-
-
This function or function block A function block groups an algorithm and a set of private data. It has inputs and outputs. returns cached data.
See Program a Multi-Core Controller.
- Returns TRUE if the internal generator axis is ready.
- See Axis Function Examples.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLAxisGenIsRdy(PipeNetwork.Axis1 );
See Also