MLAxisIsTrigged
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Verifies if the axis received a trigger event.
Inputs
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE when the function successfully executes. |
Remarks
Returns TRUE if the Fast Input event has been triggered and not yet been reset New start of the microprocessor..
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLAxisIsTrigged (PipeNetwork.Axis1, 0,1 ) ;
See Also