Block
Name |
Description |
Creates a new Pipe Block object. |
|
Verifies if a Pipe Block currently has a function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. running. |
|
Gets the value of the period Motor systems having a reciprocating or oscillating motor that operates synchronously with the periodicity of the source which supplies the electrical energy. The period of execution of a pipe is the time spent between two successive computations of set values for the same pipe. The period of execution of a pipe is specified by the PERIOD parameter of the input pipe block. of a block in user units. |
|
Gets the output value of a selected Pipe Block. |
|
Sets the value of the period of a block in user units. |