MLCompInit
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Initializes a comparator Pipe Block with user-defined settings for use in a PLC Programmable Logic Controller - A digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events. Program The act of performing a sequence of instructions or commands..
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of a created Comparator Pipe Block. |
ModuloPosition |
LREAL |
No range |
User units |
No default |
|
ThroughZero |
BOOL |
0, 1 |
N/A |
No default |
|
Reference |
LREAL |
No range |
User units |
No default |
Set the reference position in the new Comparator object. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
|
|
Returns TRUE when function starts to execute. |
Remarks
- Function block A function block groups an algorithm and a set of private data.
It has inputs and outputs. is automatically called if a Comparator Block is added to the Pipe Network.
- User-defined settings are entered in the Pipe Blocks Properties screen.
- The Transition Flag of a comparator object turns TRUE if the input position to the comparator is greater or equal to the reference.
- The Comparator Transition Flag stays TRUE until it is reset New start of the microprocessor..
- If the input ThroughZero is set to TRUE, the system must cross zero and then the reference position before the Transition Flag is set.
- If ThroughZero is FALSE, the Transition Flag is set immediately if the input pipe position is greater or equal to the Reference value.
-
-
Comparator objects are normally created in the Pipe Network using the graphical engine.
You do not have to add MLCompInit function blocks to their programs.
Parameters are entered directly The orientation components of a vector in space. in windows, and the code is then automatically added to the current project.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Initiate a created Comparator Block named “MyComp” to:
// Modulo of 360
// Require the input position to first cross 0 before the
// MLCompCheck output is triggered
// Input compared position to 45
MyComp := MLBlkCreate( 'MyComp', 'COMPARATOR' );
MLCompInit( MyComp, 360.0, TRUE, 45.0 );
See Also