MLGearReadRatSlp
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Returns the Ratio Slope value of a selected Gear Block from the Pipe Network.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of an initialized Gear object. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Slope |
LREAL |
|
1/sec (or s-1) |
The Ratio Slope value currently assigned to the selected Gear Pipe Block. This can be a different sign than what is programmed The act of performing a sequence of instructions or commands. with MLGearWriteRatSlp. |
Remarks
The Ratio Slope sets the limit in 1/Seconds (or s-1) at which step changes in Ratio are implemented.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Find the Ratio Slope value of Gear1 Pipe Block
Gear1RatioSlope := MLGearReadRatSlp(PipeNetwork.GEAR1);
See Also