MLMstForcePos
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Forces the position Position means a point in space which is described by different coordinates. Depending on the used system and transformation it can consist of a maximum of six dimensions (coordinates).This means three Cartesian coordinates in space and coordinates for the orientation. In ACS there can be even more than six coordinates. If the same position is described in different coordinate systems the values of the coordinates are different. of a Master Block to a specified position.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
EN |
BOOL |
0, 1 |
N/A |
No default |
Enables Enable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. the FB to be executed. |
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of the Master Block. |
Position |
LREAL |
No range |
User units |
No default |
Defines the Master starting position when the motion starts. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
No range |
N/A |
Returns TRUE when the function successfully executes. |
Remarks
- This block can only be executed when motion is not occurring.
- It can be used to force the master starting position to the desired values from which to start motion.
FBD Language Example
FFLD Language Example
-
-
A pulse contact is required to start the FB.
IL Language Example
Not available.
ST Language Example
//Reset New start of the microprocessor. the output position of the Master Pipe Block named “Master” to 2500.0
MLMstForcePos(PipeNetwork.Master, 2500.0);
See Also