MLMstWriteDecel
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Sets the deceleration of a master block.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
EN |
BOOL |
0, 1 |
N/A |
No default |
Enables Enable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. the FB to be executed. |
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of the Master Block. |
Deceleration |
LREAL |
No range |
User unit/sec2 |
No default |
Deceleration value expressed in user logical units per second squared. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
|
|
Returns TRUE when the function successfully executes. |
Remarks
None
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLMstWriteDecel( PipeNetwork.MASTER, 40000.0 );
See Also