MLMstWriteSpeed
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Sets the speed Speed is the absolute value of the velocity without direction. of a master block.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
EN |
BOOL |
0, 1 |
N/A |
No default |
Enables Enable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. the FB to be executed. |
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of the Master Block. |
Speed |
LREAL |
No range |
User unit/sec |
No default |
Speed of the motion. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
|
|
Returns TRUE when the function successfully executes. |
Remarks
- Set the speed of motion for the MLMstAbs and MLMstRel blocks.
- This function or function block A function block groups an algorithm and a set of private data. It has inputs and outputs. does not generate any motion.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLMstWriteSpeed( PipeNetwork.MASTER, 400.0 );
See Also