MLPmpAbs
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of a PMP function block A function block groups an algorithm and a set of private data. It has inputs and outputs. in the Pipe Network. |
Position |
LREAL |
No range |
User units |
No default |
Absolute position of the motor An actuator focused to a movement, converting electrical energy in a force or torque./load to be at after this function block is complete. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
|
N/A |
Returns TRUE if the function or function block is successfully executing. |
Remarks
- The FIRST_TRAVEL_SPEED Speed is the absolute value of the velocity without direction. is used as the velocity For a group of axes this means: In ACS the velocities of the different axes. In MCS and PCS it provides the velocity of the TCP for the motion.
- JERK In physics, jerk is the rate of change of acceleration. More precisely, the derivative of acceleration with respect to time. determines the level of parabolic acceleration.
- Returns TRUE if the function succeeded.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLPmpAbs( PipeNetwork.PmpMaster, 1000.0 ) ;
See Also