MLPhaInit
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Initializes a phaser Pipe Block.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of a phaser function block A function block groups an algorithm and a set of private data. It has inputs and outputs. in the Pipe Network. |
ModuloPosition |
LREAL |
No range |
User units |
360.0 |
|
Phase |
LREAL |
No range |
N/A |
0.0 |
Amount of phase adjustment. |
UseUserSlope |
BOOL |
0, 1 |
N/A |
Max Slope |
Determines if the Max Slope or user-defined slope is used. |
PhaseSlope |
LREAL |
No range |
User unit/sec |
0.0 |
User-defined slope for making the phase adjustment. |
StandbyValue |
LREAL |
No range |
N/A |
0.0 |
This is the output from the Phaser Block, when the pipe is active, until the MLPhaWritePhase function is executed. |
Outputs
Input |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
|
N/A |
Returns TRUE if the function or function block is successfully executing. |
Remarks
- Returns TRUE if the function succeeded.
- This function block is automatically called by the Pipe Network(MLPN_CREATE_OBJECTS) if a Phaser block is added to the Pipe Network.
- User-defined settings are entered in the Pipe Blocks Properties screen.
- The Phaser Pipe Block is assigned a Name, OUTPUT_PERIOD Motor systems having a reciprocating or oscillating motor that operates synchronously with the periodicity of the source which supplies the electrical energy. The period of execution of a pipe is the time spent between two successive computations of set values for the same pipe. The period of execution of a pipe is specified by the PERIOD parameter of the input pipe block., PHASE, PHASE_SLOPE_TYPE, and STANDBY_VALUE.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Initialize a Phaser Pipe Block named “PhaseAdjust” to a Modulo of 720, phase offset value of 30, use the Max Slope
MLPhaInit( PipeNetwork.PhaseAdjust , 720, 30, false, 30 , 10 );
See Also