MLPhaReadSlope
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Gets the phase slope value of a phaser block.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of a phaser function block A function block groups an algorithm and a set of private data. It has inputs and outputs. in the Pipe Network. |
Outputs
Input |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Slope |
LREAL |
|
User unit/sec |
Present slope value.
|
Remarks
None
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
PresentSlope :=MLPhaReadSlope( PipeNetwork.PhaseAdjust );
See Also