MLSmpConPLCAxis
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Connects a sampler block to a specific PLCopen A vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML. axis variable.
Inputs
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Default (.Q) |
BOOL |
|
N/A |
Function block is operational. |
Remarks
Figure 1: MLSmpConPLCAxis
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Connect a Sampler pipe block named “SAMPLER” to a variable named “MC_ACTUAL_POSITION” from a PLCOpen Axis named Axis1.
MLSmpConPLCAxis( PipeNetwork.SAMPLER, Axis1, MC_ACTUAL_POSITION);