Modify PLCopen Axis
- In the Project Explorer, double-click a PLCopen axis.
- Right-click the PLCopen axis in the project manager and select Properties in the menu.
Figure 1: PLCopen Axis Context Menu
The PLCopen Axis Data dialog opens:
Figure 2: PLCopen Axis Data dialog
Axis Name and Number
The PLCopen Axis Name and Number in the PLCopen Axis Data dialog are automatically applied to the PLCopen instance of an AXIS_REF structure under Global variables in the Dictionary when the project is compiled.
The PLCopen.XXXXXX_ref (MyAxis1 in this example) instance can be used in the PLC Programmable Logic Controller - A digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events. programs The act of performing a sequence of instructions or commands.:
See AXIS_REF Structure.