AXIS_REF Structure
The PLCopen A vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML. specification indicates a Structure used for identifying the axis at a function block A function block groups an algorithm and a set of private data. It has inputs and outputs. input.
AXIS_REF contains these members:
Member |
Type |
Description |
---|---|---|
AXIS_NUM |
INT |
The axis number. |
AXIS_ENGINE |
UINT |
Reserved. Do not modify this variable or rely on its value. |
See Modify PLCopen Axis about Axis Number.
You have to create and initialize this data structure in your application.