hyster
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
XIN1 |
REAL |
|
|
|
First input. |
XIN2 |
REAL |
|
|
|
Second input. |
EPS |
REAL |
|
|
|
Hysteresis. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
BOOL |
|
|
Detected hysteresis: TRUE if XIN1 becomes greater than XIN2+EPS and is not yet below XIN2-EPS. |
Remarks
- The hysteresis is detected on the difference of XIN1 and XIN2 signals.
FBD Language Example
FFLD Language Example
- In the FFLD Language, the input rung (EN) is used for enabling Enable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set.
Both are required for enabling the drive. the block.
- The output rung is the Q output.
- The block is not called if EN is FALSE.
IL Language Example
(* MyHyst is a declared instance of HYSTER function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. block *)
Op1: CAL MyHyst (XIN1, XIN2, EPS)
FFLD MyHyst.Q
ST Structured text - A high-level language that is block structured and syntactically resembles Pascal. Q
ST Language Example
(* MyHyst is a declared instance of HYSTER function block. *)
MyHyst (XIN1, XIN2, EPS);
Q := MyHyst.Q;
See Also