RS
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
SET |
BOOL |
|
|
|
Condition for forcing to TRUE. |
RESET1 |
BOOL |
|
|
|
Condition for forcing to FALSE. Highest priority command. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
BOOL |
|
|
Output to be forced. |
Remarks
- The output is unchanged when both inputs are FALSE.
- When both inputs are TRUE, the output is forced to FALSE. (reset dominant)
Truth Table
SET |
RESET1 |
Q1 prev |
Q1 |
---|---|---|---|
0 |
0 |
0 |
0 |
0 |
0 |
1 |
1 |
0 |
1 |
0 |
0 |
0 |
1 |
1 |
0 |
1 |
0 |
0 |
1 |
1 |
0 |
1 |
1 |
1 |
1 |
0 |
0 |
1 |
1 |
1 |
0 |
FBD Language Example
FFLD Language Example
IL Language Example
(* MyRS is declared as an instance of RS function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. block *)
Op1: CAL MyRS (SET, RESET1)
FFLD MyRS.Q1
ST Q1
ST Language Example
(* MyRS is declared as an instance of RS function block *)
MyRS (SET, RESET1);
Q1 := MyRS.Q1;
See Also