SR
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
SET1 |
BOOL |
|
|
|
Condition for forcing to TRUE. Highest priority command. |
BOOL |
|
|
|
Condition for forcing to FALSE. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
BOOL |
|
|
Output to be forced. |
Remarks
- The output is unchanged when both inputs are FALSE.
- When both inputs are TRUE, the output is forced to FALSE. (set dominant)
Truth Table
SET1 |
RESET |
Q1 prev |
Q1 |
---|---|---|---|
0 |
0 |
0 |
0 |
0 |
0 |
1 |
1 |
0 |
1 |
0 |
0 |
0 |
1 |
1 |
0 |
1 |
0 |
0 |
1 |
1 |
0 |
1 |
1 |
1 |
1 |
0 |
1 |
1 |
1 |
1 |
1 |
FBD Language Example
FFLD Language Example
- The SET1 command is the rung.
- The rung is the output.
IL Language Example
(* MySR is declared as an instance of SR function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. block *)
Op1: CAL MySR (SET1, RESET)
FFLD MySR.Q1
ST Q1
ST Language Example
(* MySR is declared as an instance of SR function block *)
MySR (SET1, RESET);
Q1 := MySR.Q1;
See Also