DTGetNTPSync
Function Block A function block groups an algorithm and a set of private data. It has inputs and outputs. - Read the NTP synchronization Combines an axis or axes group (as slave) with an axis as master. The slave executes its path with synchronization to the progress of the master. This is linked to a one dimension source for synchronization. enable Enable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. state.
This function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. block is specific for PCMM2G only.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
Execute |
BOOL |
TRUE, FALSE |
N/A |
No default |
If TRUE, request to read the synchronization enable state. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Done |
BOOL |
TRUE, FALSE |
N/A |
If TRUE, the command completed successfully. |
Error |
BOOL |
TRUE, FALSE |
N/A |
If TRUE, an error has occurred. |
ErrorID |
DINT |
No range |
N/A |
Indicates the error if the Error output is set to TRUE. Error Codes
|
SynchEn |
BOOL |
TRUE, FALSE |
N/A |
The present NTP synchronization state.
|
Remarks
None
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
// read the NTP synchronization state
Inst_DTGetNTPSync( bGetNTPSync );
if Inst_DTGetNTPSync.Done then
bGetNTPSync := false;
if NOT Inst_DTGetNTPSync.Error then
bNTPSyncEnable := Inst_DTGetNTPSync.SynchEn;
else
ErrorID := Inst_DTGetNTPSync.ErrorID;
end_if;
end_if;
See Also