LoadString
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
ID |
DINT |
|
|
|
ID of the string as declared in the string table. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
STRING |
|
|
Loaded string or empty string in case of error. |
Remarks
- This function loads a
string from the active string table and stores it in a STRING variable.
- The StringTable function is used for selecting the active string table.
- The ID input (the string item identifier) is an identifier declared within the string table resource.
- You don't need to define this identifier again - the system does it for you.
FBD Language Example
FFLD Language Example
IL Language Example
Op1: LD Ladder diagram - This is a method of drawing electrical logic schematics. It is a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical rails and a series of horizontal rungs between them. ID
LoadString
ST Q
ST Language Example
Q := LoadString (ID);
See Also