StringTable
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
TABLE |
STRING |
|
|
|
Name of the Sting Table resource. Must be a constant. |
COL |
STRING |
|
|
|
Name of the column in the table. Must be a constant. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
BOOL |
FALSE, TRUE |
|
TRUE if OK. |
Remarks
- This function selects
a column of a valid String Table resource to become the active string table.
- The LoadString function always refers to the active string table.
- Arguments must:
- be constant string expressions.
- fit to a declared string table and a valid column name within this table.
- If there is only one
string table with only one column defined in the project, you do not need to
call this function.
- It is the default string table.
FBD Language Example
FFLD Language Example
IL Language Example
Op1: LD Ladder diagram - This is a method of drawing electrical logic schematics. It is a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical rails and a series of horizontal rungs between them.
'MyTable'
StringTable 'First Column'
ST Structured text - A high-level language that is block structured and syntactically resembles Pascal.
OK
ST Language Example
OK := StringTable ('MyTable', 'FirstColumn");
See Also