BlinkA
Function Block A function block groups an algorithm and a set of private data. It has inputs and outputs. - Asymmetric blinker.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
RUN |
BOOL |
FALSE, TRUE |
|
|
|
TM0 |
TIME |
|
|
|
Duration of FALSE state on output. |
TM1 |
TIME |
|
|
|
Duration of TRUE state on output. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Q |
BOOL |
FALSE, TRUE |
|
Output blinking signal. |
Remarks
- The output signal is FALSE when the RUN input is FALSE.
Time Diagram
FBD Language Example
FFLD Language Example
- In the FFLD Language, the input rung is the IN command.
- The output rung is the Q output.
IL Language Example
(* MyBlinker is a declared instance of BLINKA function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. block *)
Op1: CAL MyBlinker (RUN, TM0, TM1)
FFLD MyBlinker.Q
ST Q
ST Language Example
(* MyBlinker is a declared instance of BLINKA function block. *)
MyBlinker (RUN, TM0, TM1);
Q := MyBlinker.Q;
See Also