FileSeek
Function Block A function block groups an algorithm and a set of private data. It has inputs and outputs. - Sets the current position Position means a point in space which is described by different coordinates. Depending on the used system and transformation it can consist of a maximum of six dimensions (coordinates).This means three Cartesian coordinates in space and coordinates for the orientation. In ACS there can be even more than six coordinates. If the same position is described in different coordinate systems the values of the coordinates are different. in an open file.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
Execute |
BOOL |
0, 1 |
N/A |
No default |
On the rising edge The transition of a digital signal from low to high. AKA: positive edge., test if the end of the file is reached in a file that is open for reading. |
ID |
UDINT |
N/A |
N/A |
No default |
The ID of the open file. |
POS |
DINT |
N/A |
N/A |
No default |
Number of bytes to offset from ORG.
|
ORG |
DINT |
|
N/A |
No default |
Origin of the move.
|
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Done |
BOOL |
|
|
If TRUE, the command completed successfully. |
Error |
BOOL |
|
|
If TRUE, an error has occurred. |
ErrorID |
DINT |
|
|
Indicates the error if Error output is TRUE. See the table in Search IndexFile and TCP/IP Function Block ErrorIDs. |
Remarks
Figure 1: FileCopy
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
(* FileSeek example *)
CASE StepCounter OF
0:
(* Move to beginning of the file *)
Inst_FileSeek(TRUE, MyInputFileID, 0, SEEK_SET);
StepCounter := StepCounter + 1;
1:
Inst_FileSeek(TRUE, MyInputFileID, 0, SEEK_SET);
IF Inst_FileSeek.Done THEN
Inst_FileSeek(FALSE, 0, 0, SEEK_SET);
StepCounter := StepCounter + 1;
END_IF;
END_CASE;
See Also