Differences between MC_GrpHalt and MC_GrpStop
MC_GrpHalt and MC_GrpStop both perform a controlled motion stop of all axes in an axes group.
These are the differences between the function blocks A function block groups an algorithm and a set of private data. It has inputs and outputs..
MC_GrpHalt |
MC_GrpStop |
---|---|
MC_GrpHalt can be aborted by these other commands:
|
MC_GrpStop cannot be aborted by any other command. |
While MC_GrpHalt is active, the group state is GroupMoving. |
|
When MC_GrpHalt is complete, the group state goes to GroupStandBy. |
|
See Also