MC_GrpHalt
Function Block A function block groups an algorithm and a set of private data. It has inputs and outputs. - Performs a controlled motion stop of all axes in the group.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
Execute |
BOOL |
FALSE, TRUE |
N/A |
No default |
On the rising edge The transition of a digital signal from low to high. AKA: positive edge., the command to halt all of the axes in the group is initiated. |
AxesGroup |
No range |
N/A |
No default |
The axes group the axes are stopped in. |
|
Deceleration |
LREAL |
0 < Deceleration |
N/A |
No default |
The path Set of continuous positions and orientation information in multi-dimensional space. Geometrical description of a space curve that the TCP of an axesgroup moves along. deceleration rate for all axes in the group. |
Jerk |
LREAL |
0 ≤ Jerk |
N/A |
No default |
Not supported. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Done |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command completed successfully. |
Busy |
BOOL |
FALSE, TRUE |
N/A |
TRUE from the moment the EXECUTE input is TRUE until the halt is complete. |
Active |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the halt is still executing. |
CommandAborted |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command was aborted by another function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. block. |
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
ErrorID |
INT |
-32768 to +32767 |
N/A |
Indicates the error if Error output is TRUE. |
Remarks
-
- This function block starts a motion-related action and stores data for calculations and error checking.
See Call Function Blocks Multiple Times in the Same Cycle if using a dual-core controller.
- MC_GrpHalt can be aborted.
- When the path velocity For a group of axes this means: In ACS the velocities of the different axes. In MCS and PCS it provides the velocity of the TCP reaches 0 (zero):
- Any queued moves are flushed from the buffer.
- The Done output is set.
- The state transitions to GroupStandby.
- MC_GrpHalt does NOT prevent:
- A single axis from executing.
- Other Coordinated Motion moves from executing once MC_GrpHalt has completed.
- See Differences between MC_GrpHalt and MC_GrpStop.
- See Coordinated Motion, the top-level topic for Coordinated Motion.
- See Function Blocks - General Rules about how inputs and outputs work.
Figure 1: MC_GrpHalt
FBD Language Example
FFLD Language Example
IL Language Example
BEGIN_IL Instruction list - This is a low-level language and resembles assembly. CAL Inst_MC_GrpHalt ( EnableHalt, Group1_Ref, Deceleration, Jerk ) END_IL
ST Language Example
Inst_MC_GrpHalt ( EnableHalt, Group1_Ref, Deceleration, Jerk );
See Also