Initialize and Start a Pipe Network
The Motion State Machine The complete assembly of all connected parts or devices, of which at least one is movable. is driven by the IEC International Electrotechnical Commission - A not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies. 61131-3 application with the help of dedicated function blocks A function block groups an algorithm and a set of private data. It has inputs and outputs..
Figure 1: Motion State Machine
Each arrow represents a transition from one State to another one.
To start a Pipe Network in an IEC 61131-3 application program The act of performing a sequence of instructions or commands., these steps must be performed with their respective functions A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances.:
Step |
ML Function Block |
Description |
---|---|---|
|
||
Profiles |
Create Cam Profiles from cam files. |
|
3. Create Pipe Network |
Pipe Network |
|
|
||
5. Power on all axes |
Pipe Network |
|
6. Activate the pipes |
Pipe Network |
|
7. Connect the axes to the pipes |
Pipe Network |
Example: In this Pipe Network, the function connects the Converter blocks (CNV1, CNV2 and CNV3) to the Axis blocks: |
See click here... for more information about all ML function blocks related to motion