AOUT.VALUEU
Description
AOUT.VALUEU reads/writes the analog output value when AOUT.MODE = 0 (analog output signal is determined by the user).
General Information
Type |
R/W Parameter |
Units |
V |
Range |
–10 to +10 V |
Default Value |
0 |
Data Type |
Float |
Start Version |
M_01-00-00-000 |
Variants Supported
*In SynqNet A digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices., a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.