DRV.EMUEMTURN

Description

When the emulated encoder output (EEO) is configured to generate an absolute index pulse (DRV.EMUEMODE is 2, 7 or 9) this parameter and DRV.EMUEZOFFSET define the location of the Z pulse. DRV.EMUEMTURN is used to define which turn of the position range the Z pulse is located. DRV.EMUEZOFFSET is used to define the position of the Z pulse within one revolution.

Note: If you are using multi-turn or single tune absolute feedback devices the Z pulse from generated by the EEO will always be aligned with the same mechanical position of the of the primary feedback position. If you are using an incremental feedback device then the origin of the primary feedback is not at the same mechanical position each time the drive powers up.

General Information

Type

R/W Parameter

Units

revolutions

Range

0 to 4,294,967,295

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

3491h/0

M_01-00-00-000

Related Topics

DRV.EMUEMODE, DRV.EMUERES