DRV.ICONT
Description
DRV.ICONT returns the drive In electrical engineering, a drive is an electronic device to provide power to a motor or servo. Control device for regulating the speed, torque and position of a motor. A unit controlling a motor using the current and timing in its coils. continuous rated current in Arms.
General Information
Type |
R/O Parameter |
Units |
Arms |
Range |
N/A |
Default Value |
N/A |
Data Type |
Float |
Start Version |
M_01-00-00-000 |
Index Zero pulse (zero signal) of a hardware pin such as digital input or feedback pin./Subindex | Object Start Version |
---|---|
5083h/0 |
M_01-00-00-000 |