DRV.IPEAK
Description
DRV.IPEAK returns the drive peak rated current in Arms.
General Information
Type |
R/O Parameter |
Units |
Arms |
Range |
N/A |
Default Value |
N/A |
Data Type |
Float |
Start Version |
M_01-00-00-000 |
Variant | Supported |
---|---|
MKD EtherCAT | Yes |
AKD-N | Yes |
MKD-N | Yes |
MKD-C | Yes |
Index/Subindex | Object Start Version |
---|---|
5084h /0 |
M_01-00-00-000 |