Function Block Diagram (FBD) Editor
- The editor supports advanced graphic features such as drag-and-drop, object resizing, and connection line routing features to rapidly and freely arrange the elements of a diagram.
- Insert in an FBD diagram graphic elements of the FFLD (Ladder Diagram) language (e.g., contacts and coils).
FBD Diagram Components |
Related Sections |
---|---|
Selecting and entering variables and FB instances
|
|
FFLD Components |
|
|
-
-
When a contact or a coil is selected, press the Spacebar to change its type (e.g., normal, negated, pulse When the step gets activated, the action is activated for a single execution, and possibly once again when the step is deactivated.).
Boolean connections can be negative at the entry of a block.
- Select the Boolean connection
Connections in FBD Programs The act of performing a sequence of instructions or commands.
- Press the Spacebar (a small circle is displayed)
Execution order can be displayed.