Free Form Ladder Diagram (FFLD) Editor
- Free drawing and arrangement of FFLD items.
- Supports these advanced graphic features:
See Also
Advanced Graphic Features
Change Ladder Diagram Size
Color-coded Functions
- Functions and Function Blocks A function block groups an algorithm and a set of private data. It has inputs and outputs. are color-coded as blue.
- Sub-programs and Kollmorgen UDFBs are black.
Coordinate-based Positions
Select the Entire Ladder Diagram
Split Window Capability
Allows multiple views of the same ladder program The act of performing a sequence of instructions or commands. to be displayed simultaneously.
Drag the two splitters located in the vertical and horizontal scroll bars to organize the windows.
FFLD Diagram Components |
Related Sections |
---|---|
-
-
When a contact or a coil is selected, you can press the Spacebar to change its type (normal, negated, pulse When the step gets activated, the action is activated for a single execution, and possibly once again when the step is deactivated.)