Programming Languages
These are the available programming The act of performing a sequence of instructions or commands. languages of the IEC International Electrotechnical Commission - A not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies. 61131-3 standard:
- Free Form Ladder Diagram (FFLD)
- Function Block Diagram (FBD)
- Instruction List (IL)
- Sequential Function Chart (SFC)
- Structured Text (ST)
A language must be selected for each program or User-Defined Function Block of the application.
-
- When using FBD or FFLD languages, review Use ST Expressions in Graphic Language.
See these pages about the IEC 61131-3 programming languages: