Arrays
To declare an array, enter the number of elements in the Dim. column on the Variables tab.
See Create Variables for the procedure.
For a multi-dimensional array (arrays have a maximum of three dimensions), enter the number of elements for each dimension separated by commas:
- Using 2,10,4 as the 3D array:
- The first dimension has 2 elements.
- The second dimension has 10 elements.
- The third dimension has 4 elements.
Arrays are accessed by variable indices.
myArray[myIndex1, myIndex2]
-
-
All indexes Zero pulse (zero signal) of a hardware pin such as digital input or feedback pin. are 0 based.
Example: In a single dimension array, the first element is always identified by ArrayName[0].