Download AKD PDMM Drive Firmware

Component Firmware Version Download
800MHz AKD PDMM Drive FW AKD-M-MCEC-VFirmRev, adjust in target-00-003.i00
1.2GHz AKD PDMM Drive FW AKD-M-M1EC-VFirmRev, adjust in target-00-003.i00

To upgrade AKD PDMM drive Firmware with KAS IDEClosed"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger, continue from the previous procedure as follows:

  1. In the toolbar, deactivate the Online Configuration Mode
  2. Select the drives requiring the same firmware version to be updated
    (Note that the FW download is limited to 16 drives at a time)

    • Please note that the firmware download is limited to 16 drives at a time.

  3. Click Upgrade Firmware button

    • Give careful attention to any warning dialog that appears at this point. These warnings usually include important information about preventing damage to the drives.

  4. Browse to select the new AKD/AKD2G firmware file
  5. Click Open to start the updating procedure