Call Functions or Function Blocks

When finalized, you can drag-and-drop UDFBs from the library in the (Project) node to a program just like any other function block. A new instance is automatically created.

Create an Instance of UDFB in a Program

Figure 4-98: Create an Instance of UDFB in a Program

See also: