Import a Control Panel

Control Panels may be exported and imported for easy reuse across projects. Any variables associated with the control panel will be preserved across projects.

  1. Right-click on Controller in the Project View and select Import Control Panel.
  2. Locate a saved .GRA file and click Open.
    • If the panel you are trying to import has the same name as an existing panel, you will be prompted to change the name or cancel the import.
  3. Upon clicking Open (or OK) the panel will be placed in the Project View.

See also: Export a Control Panel