AIN.OFFSET

Description

AIN.OFFSET sets the analog offset, which is added to the analog input command to the drive.  This value compensates for the analog input signal (AIN.VALUE ) offset or drift.

General Information

Type

NV Parameter

Units

V

Range

–10 to +10 V

Default Value

0 V

Data Type

Float

See Also

AIN Parameters , AIN.ZERO

Start Version

M_01-00-00-000

Variants Supported

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5003h/0

M_01-00-00-000

Related Topics

Analog Input (pg 1)

AIN.ZERO

Block Diagram for Position/Velocity Loop